About the LICELL PIN when not using RTC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the LICELL PIN when not using RTC

Jump to solution
2,215 Views
george
Senior Contributor II

Dear all,

When using i.MX6 and MMPF0100 together like i.MX6-SDP and the RTC function is unnecessary, should the LICELL pin of PMIC be open?

Or is it necessary to tie to the power supply of suitable voltage?

Best Regards,

George

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
2,062 Views
igorpadykov
NXP Employee
NXP Employee

Hi George

when not used, it should be bypassed with 0.1uF as suggests

AN4717 AN4717, Schematic Guidelines for the MMPF0100

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,063 Views
igorpadykov
NXP Employee
NXP Employee

Hi George

when not used, it should be bypassed with 0.1uF as suggests

AN4717 AN4717, Schematic Guidelines for the MMPF0100

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,062 Views
george
Senior Contributor II

Dear igor,

Thanks.

0 Kudos
Reply