About specifications of REF_CLK generated internally with i.MX6SoloLite

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About specifications of REF_CLK generated internally with i.MX6SoloLite

跳至解决方案
1,293 次查看
yuuki
Senior Contributor II

Dear all,

Would you tell me the specifications of REF_CLK generated internally?

We think about the configuration that REF_CLK is output by FEC_REF_CLK pin.
This is configuration explained in Figure 11-3 of IMX6SLHDG.

IMX6SLHDG.pdf (Rev1)
http://cache.freescale.com/files/32bit/doc/user_guide/IMX6SLHDG.pdf
- Figure 11-3. Internal reference clock(P.106)

We want to know the contents similar to specifications explained in "Table 52.RMII Signal Timing" of the data sheet.

IMX6SLCEC.pdf (Rev3)
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SLCEC.pdf
- Table 52. RMII Signal Timing(P.65)
(We understand that it is a timing specification of REF_CLK when it is input to FEC_TX_CLK pin.)

Best Regards,
Yuuki

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,213 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Strictly speaking, jitter or accuracy parameters of internal PLLs are not specified.

The only specified parameters may be found in the Datasheet(s) in section “PLL’s
Electrical Characteristics”. 
Nevertheless, we can refer to Table 1-14 (24 MHz crystal
tolerance guidelines) of the Hardware Development Guide, assuming stability (thermal,
voltage and other) of PLL output clock is fully defined by external crystal / oscillator,
and i.MX6 meets USB, PCIe, Ethernet clock specs. 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,214 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Strictly speaking, jitter or accuracy parameters of internal PLLs are not specified.

The only specified parameters may be found in the Datasheet(s) in section “PLL’s
Electrical Characteristics”. 
Nevertheless, we can refer to Table 1-14 (24 MHz crystal
tolerance guidelines) of the Hardware Development Guide, assuming stability (thermal,
voltage and other) of PLL output clock is fully defined by external crystal / oscillator,
and i.MX6 meets USB, PCIe, Ethernet clock specs. 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复