About offset 0x017C register of HS-USB Register of i.MX51

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About offset 0x017C register of HS-USB Register of i.MX51

Jump to solution
3,091 Views
yuuki
Senior Contributor II

Dear  All,

In FSL WindowsBSP,
We have the problem that a CPU may be hung-up, when a register is written by USB Driver.

When a USB driver writes any value into offset 0x017C of HS-USB register, this problem may occur.

In the source code of WinCE BSP, this register is defined as ENDPTNAKEN.

However, in a reference manual, this 0x017C register is "reserved".

MCIMX51 Multimedia Applications Processor Reference Manual Rev. 1 2/2010
- Table 60-28. HS-USB Register Summary(P.2882)

In Linux BSP source code, this 0x017C register is not defined.

In WinCE,
What kind of function does this 0x017C register have?
Is access(writing) to this 0x017C register required?


Best Regards,
Yuuki

Labels (1)
0 Kudos
Reply
1 Solution
2,967 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
8 Replies
2,968 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
2,968 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

please look below for description,

I think its usage is optional

Pic1.jpg

Pic2.jpg

Pic3.jpg

Best regards

igor

0 Kudos
Reply
2,968 Views
yuuki
Senior Contributor II

Dear Igor-san,

Thank you for your support.

Are there any limitations about writing in these fields?
If access to this register is deleted, does a problem occur?

We want to know how to prevent the hang-up of CPU.

Best Regards,
Yuuki

0 Kudos
Reply
2,968 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

access to this register is performed in

..COMMON_FSL_V2/USBD/COMMON/pdd.c

do you mean that this piece of code is not working ?

Also this register is defined in i.MX53 RM IMX53RM

sect.77.6.30 Endpoint Nake Enable (USB_UOG_ENDPTNAKEN)

Best regards

igor

0 Kudos
Reply
2,968 Views
yuuki
Senior Contributor II

Dear Igor-san,

Thank you for your support.

> do you mean that this piece of code is not working ?
=>
No.

When it is accessed this register, a CPU may be hung up.
We are looking for this root cause and workaround.

Best Regards,
Yuuki

0 Kudos
Reply
2,968 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

I think answer depends on what do you mean

by "accessed this register" - what method are you using.

Since USB driver is high speed driver, accessing its registers

as not allowed at runtime - this violates USB driver timings, they have

strict timing constraints.

I think you can write own standalone code (without OS) like

On-Board Diagnostic Suit for the i.MX53 Quick Start Board

and try to access these registers.

~igor

2,968 Views
yuuki
Senior Contributor II

Dear Igor-san,

Thank you for your support.

> I think answer depends on what do you mean
> by "accessed this register" - what method are you using.
=>
The driver in FSL_WinCE6.0 BSP for i.MX51EVK has accessed to the register.


Does standalone code for i.MX51EVK exist?
Would you send it, if you have it?

Best Regards,
Yuuki

0 Kudos
Reply
2,968 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

sorry, there is no official standalone code for i.MX51EVK

but you can request unofficial creatng SR ticket.

~igor

0 Kudos
Reply