Dear all,
Our customer wants to connect FPGA which has a 256MByte spatial area to one CS of EIM.
According to the reference manual, the following contents are listed.
IMX6DQRM.pdf (Rev2):
22.1.1 Features(P.1007)
"26-bit external address bus, max memory size can be 128 MByte (1 Gigabit)."
However, according to the datasheet, there is 32bit mode.
IMX6DQIEC.pdf (Rev3):
Table 35. EIM Internal Module Multiplexing (P.48)
In this case I think that 256MByte is supported.
2^26 *4 byte =256MByte
Can FPGA of 256MByte spatial area be connected to one CS?
May I have advice?
Best Regards,
Yuuki
已解决! 转到解答。
Hi yuuki
answer no, since total address space size is 128 MByte
according to description of ADDRSxx in IOMUXC_GPR1 register.
IMX6DQRM i.MX 6Dual/6Quad Applications Processor Reference Manual.
It also shows memory size allocation per cs.
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi yuuki
answer no, since total address space size is 128 MByte
according to description of ADDRSxx in IOMUXC_GPR1 register.
IMX6DQRM i.MX 6Dual/6Quad Applications Processor Reference Manual.
It also shows memory size allocation per cs.
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------