Hi shalini
you are right, not all ltib packages may be compiled.
pdk2009_12_mx35_Linux_RM.pdf shows allowable selections.
So you should carefully check all dependecies and fix them package by package.
I do not think that there is universal fix, which would solved all build problems.
One can look at pdk2009_12_imx35_Linux_HelloWorld_AN.pdf
IMX35_PDK0912_LINUXDOCS_BUNDLE 
it shows how to add new application to ltib. For package procedure is
similar. Note one needs to use latest i.MX35 official Freescale BSP:
L2.6.31_09.12.01_SDK_SOURCE
: Linux 2.6.31 Source Code Files 2009.12
Release support i.MX23, i.MX25, i.MX35, i.MX51
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------