About installing additional packages in ltib

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About installing additional packages in ltib

1,156 Views
shalinikp
Contributor II

M able to build Kernel image from ltib for imx35 board on Ubuntu 12.04 host. But when i try to select additional packages than the default selected ones, The packages are not building as ltib pkgs do not contain them. It tries to search from INTERNET but fails, though INTERNET connection is fine. Please help if anyone know about the issue. M stuck badly.


Labels (1)
0 Kudos
Reply
1 Reply

1,004 Views
igorpadykov
NXP Employee
NXP Employee

Hi shalini

you are right, not all ltib packages may be compiled.

pdk2009_12_mx35_Linux_RM.pdf shows allowable selections.

So you should carefully check all dependecies and fix them package by package.

I do not think that there is universal fix, which would solved all build problems.

One can look at pdk2009_12_imx35_Linux_HelloWorld_AN.pdf

IMX35_PDK0912_LINUXDOCS_BUNDLE

it shows how to add new application to ltib. For package procedure is

similar. Note one needs to use latest i.MX35 official Freescale BSP:

L2.6.31_09.12.01_SDK_SOURCE : Linux 2.6.31 Source Code Files 2009.12

Release support i.MX23, i.MX25, i.MX35, i.MX51

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply