About image converter.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About image converter.

1,181 次查看
takashitakahash
Contributor III

Description of IMX6SDL RM of sect 38.4.5.2 Processing tasks.

  there are describe on below.

  Each of the three processing sections performs up to three processing tasks with time sharing:

  1. .Preprocessing task for encoding.
  2. .Preprocessing task for displaying image from sensor (viewfinder).
  3. .Postprocessing task.

I did not understand well the meaning of each contents.

For example, Down sizing section, above 1 ~3  is what process is specifically for.

Then, if BT.656 CVBS signal is input, please teach me the process specific examples of items 1-3 above.

标签 (2)
0 项奖励
回复
1 回复

1,106 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

"Down sizing section" also may have up to

three processing tasks with time sharing:

1. Preprocessing task for encoding.

2. Preprocessing task for displaying image from sensor (viewfinder).

3. Postprocessing task.

Table 38-21. IC's DMA Channels shows available data transfers IMX6SDLRM

for all these 3 Tasks. All Tasks can perform CSC as shown on Table 38-20. IC Parameters

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------