About iMX6SX DDR Code alias

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About iMX6SX DDR Code alias

ソリューションへジャンプ
2,846件の閲覧回数
mileswang
Contributor II

Hello,

I read the IMX6SXRM (i.MX 6SoloX Applications Processor Reference Manual)

At page 196, there is a line:

1000_0000 1FFF_7FFF 256 MB -64 KB DDR Code alias

Whose alias is it? What is the start address?

Thanks,

Miles

ラベル(1)
0 件の賞賛
返信
1 解決策
2,562件の閲覧回数
Yuri
NXP Employee
NXP Employee

  For CM4 :

DDR address space is 0x8000_0000 – 0xDFFF_FFFF

and its alias :

0x1000_0000 - 0x1FFF_7FFF,

where 0x8000_0000 corresponds 0x1000_0000

Regards,

Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,562件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Really address range 0x1000_0000 – 0xFFFF_FFFF is reserved for DDR memory.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,562件の閲覧回数
mileswang
Contributor II

Dear Yuri,

Sorry. I don't understand your answer. Below is a part of the CM4 memory map:

cm4.png

I can understand "OCRAM_S Aliased" is the alias of OCRAM_S. They are pointer to same memory region.

Then who is the alias of "DDR Code alias" (1000_000 to 1FFF_7FFF)?

Thanks,

Miles

0 件の賞賛
返信
2,563件の閲覧回数
Yuri
NXP Employee
NXP Employee

  For CM4 :

DDR address space is 0x8000_0000 – 0xDFFF_FFFF

and its alias :

0x1000_0000 - 0x1FFF_7FFF,

where 0x8000_0000 corresponds 0x1000_0000

Regards,

Yuri.

0 件の賞賛
返信