About iMX28 secure boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About iMX28 secure boot

1,072 次查看
liuxing
Contributor II

Hi All,

   I have some questions about the secure boot of iMX28.

1. about boot csf file

# Base address of the binary file, Offset of the block within the binary file,
Length of block in bytes, binary file name
[Authenticate Data]
Verification index = 2
Engine = DCP
Blocks = 0x41008000 0x0 0x2A000 "u-boot_pad.bin"

pastedImage_1.png

Beause we use the WinCE platform,How to calculate the xldr binary offset address within the ivt binary file?

the eboot bd file:

options {
driveTag = 0x00;
flags = 0x01;
}

constants {
xldr_addr = 0x00000004;
eboot_addr = 0x40050000;
bmp_addr = 0x40094000;
ivt_addr = 0x8000;
}

sources {
xldr = "xldr.nb0";
eboot = "eboot.nb0";
bmp = "splash_eboot.bmp";
}

section (0) {
load xldr > xldr_addr;
load ivt (entry = xldr_addr) > ivt_addr;
hab call ivt_addr;

load bmp > bmp_addr;

load eboot > eboot_addr;
load ivt (entry = eboot_addr) > ivt_addr;
hab call ivt_addr;
}

2.The SEC_CONFIG has been mentioned many times in AN4555 file.However,I can't find any detailed description about it.And how can we change this register when we want to debug the fuse configuration?

标签 (1)
0 项奖励
回复
1 回复

1,024 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport
0 项奖励
回复