Hi community,
Our partner have a question about i.MX53 ENGcm11038.
Please see their questions as below.
[Q1]
Please see ENGcm22038 description in IMX53CE (Rev.5).
It says "Due to non proper clock synchronization implementation,".
Our partner want to know this issue is a problem between what clock and what clock.
Would you let me know it?
[Q2]
We understansd EMI2.5 = EIM, so we believe this errata will be not occurred when EIM is not used, right?
Or EMI includes not only EIM but also DRAM and NAND interface?
Best Regards,
Satoshi Shimoda
已解决! 转到解答。
From the team :
1> Sorry, it's an old project, and not designed by our team, so I am not able to find the information so far
2> the EMI include ddr and nand interface. So they are also impacted
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
From the team :
1> Sorry, it's an old project, and not designed by our team, so I am not able to find the information so far
2> the EMI include ddr and nand interface. So they are also impacted
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yuri,
2> the EMI include ddr and nand interface. So they are also impacted
OK, I got it.
By the way, I guess this errata is not occurred if the EIM pads is used for other function (ex. use EIM_A25 pad for GPIO instead of EIM), right?
Best Regards,
Satoshi Shimoda