About i.MX53 ENGcm11038.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About i.MX53 ENGcm11038.

Jump to solution
1,024 Views
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about i.MX53 ENGcm11038.

Please see their questions as below.

[Q1]

Please see ENGcm22038 description in IMX53CE (Rev.5).

It says "Due to non proper clock synchronization implementation,".

Our partner want to know this issue is a problem between what clock and what clock.

Would you let me know it?

[Q2]

We understansd EMI2.5 = EIM, so we believe this errata will be not occurred when EIM is not used, right?

Or EMI includes not only EIM but also DRAM and NAND interface?

Best Regards,

Satoshi Shimoda

Labels (1)
0 Kudos
Reply
1 Solution
883 Views
Yuri
NXP Employee
NXP Employee

  From the team :

1>  Sorry,  it's an old project, and not designed by our team, so I am not able to find the information so far

2> the EMI include ddr and nand interface.  So they are also impacted


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
884 Views
Yuri
NXP Employee
NXP Employee

  From the team :

1>  Sorry,  it's an old project, and not designed by our team, so I am not able to find the information so far

2> the EMI include ddr and nand interface.  So they are also impacted


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
883 Views
satoshishimoda
Senior Contributor I

Hi Yuri,

2> the EMI include ddr and nand interface.  So they are also impacted

OK, I got it.

By the way, I guess this errata is not occurred if the EIM pads is used for other function (ex. use EIM_A25 pad for GPIO instead of EIM), right?

Best Regards,

Satoshi Shimoda

0 Kudos
Reply
883 Views
Yuri
NXP Employee
NXP Employee

Yes, GPIO is not affected.

Regards,

Yuri.