Windows Embedded Compact 7 i.MX6 Find Applications Core

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Windows Embedded Compact 7 i.MX6 Find Applications Core

1,538件の閲覧回数
kriszawada
Contributor III

I am using the Freescale SABRE MCIMX6Q-SD and Windows Embedded Compact 7 that is running two Qt applications.

Is there a way to determine within the software how many cores the OS is utilizing?

Is there a way to determine which core my applications are being executed on?

Is there a way to start my application and assign it to specific core?

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,456件の閲覧回数
Yuri
NXP Employee
NXP Employee

  I hope the following helps.

http://social.technet.microsoft.com/wiki/contents/articles/14942.smp-verification-on-wec-7-with-i-mx...


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信