About error message from V4L2 capture in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About error message from V4L2 capture in i.MX6DQ.

Jump to solution
3,601 Views
keitanagashima
Senior Contributor I

Dear All,

Hello. I have a question about the error message from V4L2 capture in i.MX6DQ.

Could you confirm this question?

[Overview]

The LCD resolution is 1280x720, so we need capture Camera video as 1280x720 via V4L2 interface.

When we capture the video, find the warning messages scroll on serial console frequently, but the capture result is OK.

Although the function seems OK, but what does the warning message means?

If width = 800,  height = 480, there is no warning "imx-ipuv3 imx-ipuv3.0: IDMAC9's EBA0 is not 8-byte aligned".

If width = 1280, height = 720, there is warning "imx-ipuv3 imx-ipuv3.0: IDMAC9's EBA0 is not 8-byte aligned".

[Question]

When width = 1280, height = 720, how to eliminate the warning?

[Related code (BSP: L3.0.35_4.1.0)]

If ((fd_output_v4l = open("video17", O_RDWR, 0)) < 0)

{

  ERROR("Unable to open %s\n", EARLY_RVC_DEV_VD_OUPTPUT);

  return -1;

}

crop.type = V4L2_BUF_TYPE_VIDEO_OUTPUT;

crop.c.top = top;

crop.c.left = left;

crop.c.width = width;

crop.c.height = height;

if (ioctl(fd_output_v4l, VIDIOC_S_CROP, &crop) < 0)

{

  ERROR("set crop failed\n");

  return -1;

}

Best Regards,

Keita

Labels (3)
0 Kudos
Reply
1 Solution
3,208 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Yes, the visual effect observed ("width = 1280, height = 720") may be concerned

with the non-aligned accesses. As has been discussed, the issue relate to Linux

memory allocation mechanism, therefore to solve it please apply to professional

service.

NXP Professional Services|NXP

Regards,

Yuri.

View solution in original post

8 Replies
3,208 Views
Yuri
NXP Employee
NXP Employee

Hello,

    According to i.MX6 RM (say, Table 37-14. Channel Parameters Memory for non-interleaved) :
The actual physical address value (of EPBA) is divided by 8 (i.e. only bits [31:3] of the actual

address are used).

  So, parameter “width” x “bytes_per_pixel” should be divisible by 8,

in order to get aligned addresses of the frame buffers. 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,208 Views
keitanagashima
Senior Contributor I

Hi Yuri,

Sorry for my delay response.

When "width = 1280, height = 720", the actual physical address value (of EPBA) is not divided by 8.

However, the way we apply the memory is as follows:

struct v4l2_requestbuffers buf_req;

buf_req.count = 4;

buf_req.type = V4L2_BUF_TYPE_VIDEO_OUTPUT;

buf_req.memory = V4L2_MEMORY_MMAP;

ioctl(fd_output_v4l, VIDIOC_REQBUFS, &buf_req);

Debugg  information is as follows :

[    5.386728] imx-ipuv3 imx-ipuv3.0: IDMAC9's EBA0 is not 8-byte aligned. addr0=403703204

[    5.557222] imx-ipuv3 imx-ipuv3.0: IDMAC9's EBA0 is not 8-byte aligned. addr0=404751780

[    5.730014] imx-ipuv3 imx-ipuv3.0: IDMAC9's EBA0 is not 8-byte aligned. addr0=405800356

[    6.107377] imx-ipuv3 imx-ipuv3.0: IDMAC9's EBA0 is not 8-byte aligned. addr0=406848932

So, I don't know how to intervene the memory address allocation can be divisible by 8.

And what to do to eliminate the warning message.

Best Regards,

Keita

0 Kudos
Reply
3,208 Views
Yuri
NXP Employee
NXP Employee

Hello,

    since standard Linux malloc() function does not provide aligned memory address,

it is needed to apply own / manual memory allocation for frame buffers.

http://stackoverflow.com/questions/1919183/how-to-allocate-and-free-aligned-memory-in-c

Regards,

Yuri.

0 Kudos
Reply
3,208 Views
keitanagashima
Senior Contributor I

Hi Yuri,

I could not find the source code which allocates these memory, please help me confirm it, and how to modify the code to make the memory can be divisible by 8?

Best Regards,

Keita

0 Kudos
Reply
3,208 Views
Yuri
NXP Employee
NXP Employee

Hello,

Perhaps, the simplest way is to comment warning in sources, assuming

there are no visible issues on the screen.

The message is located in file

  

/drivers/mxc/ipu3/ipu_param_mem.h

Regards,

Yuri.

0 Kudos
Reply
3,203 Views
keitanagashima
Senior Contributor I

Dear Yuri,

Please re-open for this topic.

When V4L2 output "width = 1280, height = 720", camera screen is splitted in the vertical middle of screen, detailed see attached files.

When "width = 800, height = 480", camera screen is normal.

So I think It's a relationship with this warning message "imx-ipuv3 imx-ipuv3.0: IDMAC9's EBA0 is not 8-byte aligned".

Please confirm this new found issue.

Best Regards,

Keita

0 Kudos
Reply
3,209 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Yes, the visual effect observed ("width = 1280, height = 720") may be concerned

with the non-aligned accesses. As has been discussed, the issue relate to Linux

memory allocation mechanism, therefore to solve it please apply to professional

service.

NXP Professional Services|NXP

Regards,

Yuri.

3,203 Views
Yuri
NXP Employee
NXP Employee

Hello,

this is general Linux issue.
I created request 00073230 for working with it.

Regards,

Yuri.

0 Kudos
Reply