About eMMC R/W Test and boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About eMMC R/W Test and boot

3,521件の閲覧回数
ysato_ad
Contributor II

Hello

I designed a custom board with reference to the i.MX8M Mini EVK.
The eMMC is connected to mmc 1.

1) Please tell me how to easily test R/W.
2) Please tell me how to boot from eMMC.

u-boot=> mmc list
FSL_SDHC: 0 (SD)
FSL_SDHC: 1 (eMMC)

u-boot=> mmc info
Device: FSL_SDHC
Manufacturer ID: 74
OEM: 4a60
Name: USD
Bus Speed: 50000000
Mode : SD High Speed (50MHz)
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 28.7 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes

u-boot=> mmc dev 1
switch to partitions #0, OK
mmc1(part 0) is current device

u-boot=> mmc info
Device: FSL_SDHC
Manufacturer ID: fe
OEM: 14e
Name: MMC02
Bus Speed: 52000000
Mode : MMC DDR52 (52MHz)
Rd Block Len: 512
MMC version 4.4.1
High Capacity: No
Capacity: 1.8 GiB
Bus Width: 8-bit DDR
Erase Group Size: 512 KiB
HC WP Group Size: 0 Bytes
User Capacity: 1.8 GiB
Boot Capacity: 1 MiB ENH
RPMB Capacity: 128 KiB ENH

ラベル(2)
0 件の賞賛
返信
1 返信

3,486件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yuichi

for programming emmc one can follow i.MX Linux User’s Guide

https://community.nxp.com/docs/DOC-343518 

or third party guidelines

https://boundarydevices.com/programming-emmc-on-i-mx8/ 

https://boundarydevices.com/zeus-yocto-release-for-i-mx8mq/ 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信