About dynamic changes in VSYNC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About dynamic changes in VSYNC

ソリューションへジャンプ
1,682件の閲覧回数
goto11
Contributor III

Hello,

 

I want to dynamically toggle between 30Hz and 60Hz for VSYNC settings.
I don't want screen tearing to occur when changing.
When should I switch the LCD PLL?


best regards
Goto

ラベル(1)
0 件の賞賛
返信
1 解決策
1,672件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Goto

 

I am afraid it is not feasible as special initialization sequence is needed when changing

timings, it is described in sect.13.2.2.7.1 Code Example to Initialize eLCDIF in VSYNC Mode

(the same is for other modes)

i.MX 7Dual Applications Processor Reference Manual

Those common initialization steps in sect.13.2.2.5 "Initializing the eLCDIF" may lead to tearing.

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,673件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Goto

 

I am afraid it is not feasible as special initialization sequence is needed when changing

timings, it is described in sect.13.2.2.7.1 Code Example to Initialize eLCDIF in VSYNC Mode

(the same is for other modes)

i.MX 7Dual Applications Processor Reference Manual

Those common initialization steps in sect.13.2.2.5 "Initializing the eLCDIF" may lead to tearing.

 

Best regards
igor

0 件の賞賛
返信