About ddr hardware calibration at imx6ull

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About ddr hardware calibration at imx6ull

610 Views
junya
Contributor IV

Hi, NXP.

I want to implement hardware calibration for DDR3 with i.mx6ull. Is there any information available?I have checked the procedure in [i.MX 6 Series DDR Calibration.pdf], but I would like to obtain the source code.

 

~Background~
We are having problems with DDR3 calibration.
There have been many cases of mass-produced products suddenly stopping and freezing.
After investigating, it seems that there is a problem between DDR3 and i.mx6ull.
When I tried calibrating with a stress tool, the MPDGCTRL0 value seems to vary.

0x0130012c ~ 0x0158148

Is this range normal? Is it abnormal?
If you set this register to the optimal value for each individual device, it will work properly.


best regards.

0 Kudos
Reply
2 Replies

514 Views
yoshi
NXP Employee
NXP Employee

Hi @junya san

I will check and back to you soon.

Best Regards
Yoshi

 
 

 

 

0 Kudos
Reply

556 Views
junya
Contributor IV

Hi, @yoshi san.

Could you please follow up this thread? 

0 Kudos
Reply