Dear Sir or Madam,
Hello.
I have a question about compiler options when using NEON in i.MX6DL.
BSP:Yocto L3.10.17_1.0.0
We are executing the program which does an image processing at high speed with NEON.
But, it didn't perform well.
When compiling a program, we sets following compiler options.
[Compiler options]
arm-poky-linux-gnueabi-gcc -march=armv7-a -mthumb-interwork -mfloat-abi=hard -mfpu=neon -mcpu=cortex-a9 -mtune=cortex-a9 --sysroot=/opt/poky/1.5.1/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi -c -O3 -flax-vector-conversions -I./../../test/header -I./../../test/header2 -I./ -I./../../../fsl-community-bsp/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/opencv/2.4.6+gitAUTOINC+c5afaa4e8d-r0/packages-split/opencv-dev/usr/include test1.c test2.c
[Quesition]
Please give me your advice to implove the performance.
PS,
When changing "mfloat-abi=hard" to "soft" or "softfp", it became a build error.
Best Regards,
Keita
已解决! 转到解答。
1.
Please refer to the next VFP introduction on i.MX6 :
https://community.freescale.com/docs/DOC-100112
Also, the following may be helpful :
"Question, enabling NEON H/W"
https://community.freescale.com/message/380469#380469
2.
Note, that under Linux we should use the same options for floating point support and
the same interface for floating point parameters in fucntion calls (ABI) : hardware or software.
Therefore if Linux release is based on hardware options, it is needed to apply those ones
to all applications.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
1.
Please refer to the next VFP introduction on i.MX6 :
https://community.freescale.com/docs/DOC-100112
Also, the following may be helpful :
"Question, enabling NEON H/W"
https://community.freescale.com/message/380469#380469
2.
Note, that under Linux we should use the same options for floating point support and
the same interface for floating point parameters in fucntion calls (ABI) : hardware or software.
Therefore if Linux release is based on hardware options, it is needed to apply those ones
to all applications.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------