About changing the default CPU frequency in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About changing the default CPU frequency in i.MX6DQ.

Jump to solution
1,732 Views
keitanagashima
Senior Contributor I

Dear All,

Hello. I have a question about changing the CPU frequency.

Now, my customer is using jb4.2.2_1.1.0 and default CPU freq is 792MHz.

We want to change the CPU freq from 792MHz to 996MHz.

We tried to change the kernel parameter from arm_freq=800 to arm_freq=1000.

But, Warning log was repeated.

- COULD NOT SET SOC VOLTAGE BACK!!!!

- COULD NOT SET PU VOLTAGE!!!!

The error was outputted at the function of "function set_cpu_freq" under 'kernel_imx/src/arch/arm/plat-mxc/cpufreq.c'.

Maybe, it looks internal LDOs setting error.

[Question]

How should one change the CPU freq in U-boot?

Best Regards,

Keita

Labels (4)
0 Kudos
Reply
1 Solution
1,387 Views
Yuri
NXP Employee
NXP Employee

Hello,

  By default the CPU FREQ is enabled and it makes sense to control frequency via

proper governor after Linux boot. In this sense the kernel boot parameter as “arm_freq=1000”

does not make sense.

Regards,

Yuri.

View solution in original post

0 Kudos
Reply
3 Replies
1,387 Views
Yuri
NXP Employee
NXP Employee

Hello,

The Android is based on i.MX 6Quad BSP L3.0.35_4.0.0 GA release.

According to Table 6 (Kernel Boot Parameters) of the “Linux Release Notes”,

by defaut, LDO bypass is enabled, assuming that external PMIC should supply

VDDARM_IN/VDDSOC_IN power rail. But looks like in Your case PMIC is absent.
   “If you want to use internal LDO, please specify " ldo_active=on" to the kernel

command line”.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,387 Views
keitanagashima
Senior Contributor I

Dear Yuri,

Hello. Thank you for your reply.

>by defaut, LDO bypass is enabled, assuming that external PMIC should supply

>VDDARM_IN/VDDSOC_IN power rail. But looks like in Your case PMIC is absent.
>   “If you want to use internal LDO, please specify " ldo_active=on" to the kernel

>command line”.

We checked the PMU_REG_CORE register and confirmed LDO enabled.

But, the error occurred.

[Q1]

Is my understanding right?

- By the setting of arm_freq=1000, automatically, the voltage of LDO isn't changed.

[Q2]

How should one change the CPU freq and LDO voltage?

Best Regards,

Keita

0 Kudos
Reply
1,388 Views
Yuri
NXP Employee
NXP Employee

Hello,

  By default the CPU FREQ is enabled and it makes sense to control frequency via

proper governor after Linux boot. In this sense the kernel boot parameter as “arm_freq=1000”

does not make sense.

Regards,

Yuri.

0 Kudos
Reply