About boot frequency of i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About boot frequency of i.MX6DQ.

Jump to solution
1,699 Views
keitanagashima
Senior Contributor I

Dear Sir or Madam,

[Q1]

Refer to Table 8-2. Boot eFUSE Descriptions in MCIMX6DQRM(Rev.2).

There is below description.

------

BT_FREQ (BOOT_CFG3[2])

0 - ARM - 792 MHz, DDR - 396 MHz, AXI -264 MHz

1 - ARM - 396 MHz, DDR - 352 MHz, AXI -176 MHz

------

Next, refer to Table 5-4. EIM Boot Fusemap in RM(Rev.2).

It was "Boot Frequencies (ARM/DDR) 0 - 792 /528 MHz"

Which description is right?

[Q2]

freescale has 2 type of i.MX6DQ auto product, 1GHz or 852MHz grade

Could you tell me a selectable BOOT frequency combination in BOOT_CFG3[2](BOOT Frequency Selection)?

(ARM / DDR / AXI)

Best Regards,

Keita

Labels (3)
0 Kudos
Reply
1 Solution
1,500 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
3 Replies
1,501 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
1,500 Views
Yuri
NXP Employee
NXP Employee

1.

  This is a misprint in our i.MX6 Reference Manual :

it is mentioned BOOT Frequency as “ARM - 792 MHz, DDR - 396 MHz”,  
but it should be  ARM - 792 MHz, DDR - 528 MHz”.

2.
Both BOOT Frequency selection options are acceptable for any of i.MX6 DQ auto

qualified parts (1 GHz and 852 MGz). 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,500 Views
keitanagashima
Senior Contributor I

Hi Yuri,

Thank you for your prompt reply!

OK. I understood ARM - 792 MHz, DDR - 528 MHz are correct at boot frequency.

Best Regards,

Keita

0 Kudos
Reply