Dear All,
Hello.
I found the difference of aclk_sel field between Reference manual and source code.
First, Refer to aCCM_CSCMR1 register in IMX6DQRM(Rev.3).
CCM_CSCMR1[aclk_sel]
00 derive clock from PLL2 PFD2
01 derive clock from pll3_sw_clk
10 derive clock from AXI
11 derive clock from PLL2 PFD0
Next, "_clk_emi_set_parent" function in arch\arm\mach-mx6\clock.c of jb4.2.2_1.1.0.
00 derive clock from AXI
01 derive clock from pll3_sw_clk
10 derive clock from PLL2 PFD2
11 derive clock from PLL2 PFD0
Which is right description?
Best Regards,
Keita
解決済! 解決策の投稿を見る。
HI Keita
right is RM, also these settings are used in latest 3.14.28 BSP clk-imx6q.c
(emi_sels)
linux-2.6-imx.git - Freescale i.MX Linux Tree
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
HI Keita
right is RM, also these settings are used in latest 3.14.28 BSP clk-imx6q.c
(emi_sels)
linux-2.6-imx.git - Freescale i.MX Linux Tree
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------