About WALAT Setting in MDMISC Register

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About WALAT Setting in MDMISC Register

1,161 Views
MasakiHayakawa
Contributor III
Hi,
We want to know whether WALAT in MDMISC is set to 1 or 0.
We executed calibration using ddr_stress_tester_v3.00, and the tool displayed the following message.
WARNING: write-leveling calibration value is greater than 1/8 CK.
 Per the reference manual, WALAT must be set to 1 in the register MDMISC(0x021B0018).
 This has been performed automatically.
 However, in addition to updating the calibration values in your DDR initialization,
 it is also REQUIRED change the value of MDMISC in their DDR initialization as follows:
    MMDC_MDMISC (0x021b0018) =  0x00011740
So we set WALAT to 1, but our system was haugup.
We set WALAT to 0, and our system was not hangup.
Please tell me your recommend setting.
Processor of our system board is i.MX6Dual.
Best Regards.
Labels (3)
0 Kudos
Reply
1 Reply

1,065 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

    Use AN4467 (i.MX 6 Series DDR Calibration); in particular - section 11 (Write Leveling)

https://www.nxp.com/docs/en/application-note/AN4467.pdf 

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos
Reply