Dear Sir or Madam,
Hello.
I have a question about USB interrupt in i.MX6SDL.
BSP:jb4.2.2_1.1.0
Board: Custom board
My customer set USB InterruptEnableRegister to usbintr=0x00000000 ( = All interrpts are disable).
However, the interrupt of SRI(bit7) and FRI(bit3) in USB StatusRegister sometimes occurs.
Is there a part which makes these interrupts enable in BSP?
Best Regards,
27-May-2014
Keita Nagashima