About USB interrupt in i.MX6SDL.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About USB interrupt in i.MX6SDL.

1,110 Views
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

I have a question about USB interrupt in i.MX6SDL.

BSP:jb4.2.2_1.1.0

Board: Custom board

My customer set USB InterruptEnableRegister to usbintr=0x00000000 ( = All interrpts are disable).

However, the interrupt of SRI(bit7) and FRI(bit3) in USB StatusRegister sometimes occurs.

Is there a part which makes these interrupts enable in BSP?

Best Regards,

27-May-2014

Keita Nagashima

Labels (4)
0 Kudos
Reply
2 Replies

975 Views
jamesbone
NXP TechSupport
NXP TechSupport

In which archive is your customer making the modification of the USBINTR register?

0 Kudos
Reply

975 Views
keitanagashima
Senior Contributor I

Hi jamebone,


>In which archive is your customer making the modification of the USBINTR register?

kernel_imx/src/drivers/usb/gadget/arcotg_udc_uq/arcotg_udc.c

My customer set the fsl_writel(0, &dr_regs->usbintr) of function dr_controller_stop.


Best Regards,

Keita


0 Kudos
Reply