About SECO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About SECO

1,718件の閲覧回数
dlliweihua
Contributor III

Dear NXP community,

I want to know what state SECO enters after boot stage?

Can I use the authentication hardware of SECO to verify my images(such as images for upgrade purpose) while the OS(linux, qnx and so on)running?

Thanks in advance.

liweihua

0 件の賞賛
返信
2 返答(返信)

1,698件の閲覧回数
Yuri
NXP Employee
NXP Employee

@dlliweihua 
Hello,

   SECO ROM provides initialization and SECO FW check,
further activity is performed by SECO FW, usually in loop.
You may look at Figure 2 (Secure boot flow overview) of
"Secure Boot on i.MX 8 and i.MX 8X Families using AHAB"
app note.
    Also use section 4.4 [Authenticating OS containers (and
other ones)].

https://www.nxp.com/docs/en/application-note/AN12312.pdf

 

Regards,
Yuri.

0 件の賞賛
返信

1,694件の閲覧回数
dlliweihua
Contributor III

@Yuri 

OK, I'll check it.

Thanks a lot!

Regards,

liweihua