About SD Card Power Down

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About SD Card Power Down

Jump to solution
1,917 Views
goto11
Contributor III

Hello,Community

As shown below, at power down, CLK, CMD and DATA must be logic 0.

For example, if you use SW_MUX_CTL_Register(IOMUXC_SW_MUX_CTL_PAD_SD1_CLK) for ALT0_SD1_CLK and use it as a clock, do you have to perform the following processing at power down?

Or can the program force a logical 0 to be output?

1.Change the allocation to 100kPD(IOMUXC_SW_PAD_CTL_PAD_SD1_CLK).
2. Change the allocation to ALT5_GPIO5_IO3(IOMUXC_SW_MUX_CTL_PAD_SD1_CLK).
3. Assign to input with GPIOx_GDIR.

pastedImage_1.png

best regards

Goto

Labels (1)
0 Kudos
Reply
1 Solution
1,871 Views
igorpadykov
NXP Employee
NXP Employee

Hi GoTo

you are right, one can force signals to logical 0 in software

using your sequence.


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,872 Views
igorpadykov
NXP Employee
NXP Employee

Hi GoTo

you are right, one can force signals to logical 0 in software

using your sequence.


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply