About Read DQS Calibration.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About Read DQS Calibration.

Jump to solution
3,121 Views
keitanagashima
Senior Contributor I

Dear All,

Hello.

I have a question about Read DQS Calibration.

Refer to attached file.

Could you check my understanding?

Best Regards,

Keita

Labels (4)
0 Kudos
Reply
1 Solution
2,930 Views
LPP
NXP Employee
NXP Employee

I'm not sure about the values obtained from the DDR Stress Tester but your consideration is correct. This value of DG_HC_DEL0=3 represents Gate delay of 1.5 clocks.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,931 Views
LPP
NXP Employee
NXP Employee

I'm not sure about the values obtained from the DDR Stress Tester but your consideration is correct. This value of DG_HC_DEL0=3 represents Gate delay of 1.5 clocks.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply