About RT1170 dual-core boot problem: cm7 kernel loading cm4 image to RAM implicit loading method

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About RT1170 dual-core boot problem: cm7 kernel loading cm4 image to RAM implicit loading method

10,915件の閲覧回数
liuhailong
Contributor III

 

Hello, @Pavel_Hernandez in my company's project, I have encountered two thorny issues during my recent development work. I hope you can provide some answers instead of just providing a link to the article. Thank you

  1. Consultation on CM7 Core Guidance and CM4 Core Issues (Consultation on Dual Core Launch Issues)

Tool used: MCUXPRESSO

Processor used: RT1170

Reference docu¥ment: AN13264

liuhailong_1-1695627661513.png

My requirement is to CM7 core loading CM4 core image to run in RAM. As mentioned in the underlined part of the figure, when the development tool is MCU XPRESSO, load implicitly, similar to initialize some variables in RAM. What initial variables and methods are used? I am basically completely unfamiliar with this method. Can you provide a detailed explanation about this loading method?

2.Is there any specific process and method for porting our company's projects to FREE RTOS in the MCU XPRESSO tool that can be referenced?

iMXRT1170 

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

10,600件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I apologize for the late response, I was researching more information about these questions, and thanks for being clear on the pdf in addition to this I exposed your case to my team to get more details and from here the following questions arise.

What are the requirements for running in RAM? I mean there are some types of RAMs.

Pavel_Hernandez_0-1696872095845.png

Do you know at what address in RAM want to work with?
Could you elaborate further about what you want to achieve with your application?

Best regards,
Pavel

0 件の賞賛
返信

10,869件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I´m Pavel, and I will be supporting your case, let me get into your case and when I have more information, I will contact you.

0 件の賞賛
返信

10,652件の閲覧回数
liuhailong
Contributor III

@Pavel_Hernandez Do you have the latest explanations and follow-up on the questions I asked?

0 件の賞賛
返信

10,651件の閲覧回数
liuhailong
Contributor III

@Pavel_Hernandez Do you have the latest explanations and follow-up on the questions I asked?

0 件の賞賛
返信

10,829件の閲覧回数
liuhailong
Contributor III

Regarding CM7 core loading CM4 core, can we use the method of displaying loading in KEIL in MCUXPRESSO through fsl_incbin.S assembly file,Compile cm4 image bin file into cm7 image。My analysis is:Keil and MCUXPRESSO are very different , loading method is not necessarily applicable

0 件の賞賛
返信

10,844件の閲覧回数
liuhailong
Contributor III

Hello, thank you for your hard work. This is the latest supplement to my question. I introduced my thoughts on this question in detail. I hope my thoughts can be verified and confirmed

0 件の賞賛
返信