About QuadSPI configuration parameter description

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About QuadSPI configuration parameter description

ソリューションへジャンプ
1,601件の閲覧回数
eishishibusawa
Contributor III

Dear Sir

 

I refer to the IMX6ULLRM Rev.1.

I want to confirm the value in Table 8-23.

 

Name : Hold Delay

Value : QSPI1 B : QSPI1 A = 01 : Disable : Enable

Q1.

Is this value a binary number?

(Value 01 <- 2b01 ?)

 

Name : Serial Clock Frequency

Value : Clock = 06 : 99 MHz (only SDR mode)

Q2.

Is this value a decimal number?

 

Name : Mode of operation of serial Flash

Value : Mode = 01 : Single

Q3.

Is this value a decimal number?

 

Best Regards,

Eishi SHIBUSAWA

 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,540件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Eishi

1.  yes

2.  yes

3.  yes

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,541件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Eishi

1.  yes

2.  yes

3.  yes

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信