Hello,
I am designing a circuit with DDR mode with internal sampling with Quad SPI.
I have two questions.
No1
The following is described in the NOTE of 10.2.12 Output timing in DDR mode of i.MX 7Dual Applications Processor Reference Manual.
Where is TX_DDR_DELAY_EN the Field of the register?
TX_DDR_DELAY_EN should be set to 1 for DDR mode.
No2
The Serial Clock Frequency in Table 6-50 (Quad SPI configuration parameters) can be set up to 76 MHz in DDR mode.
The half cycle of 76MHz is 6.57ns. ((1 / 76MHz) / 2)
On the other hand, the TIS of Table 82 (Quad SPI Input / Read Timing) of the data sheet states that it is min 8.67ns.
Since the half cycle of 76MHz is shorter than 8.67ns, can't it be used at 76MHz?
Is my way of thinking wrong?
best regards
Goto