Hi Yuri,
Thank you for your reply.
> App note AN5113 (Powering an i.MX 6SL Based System Using
>the PF3000 PMIC) provides recommended configuration in Table 2 (PF3000 + i.MX 6SL
>Power Tree), assuming LPDDR2 (preprogrammed A5 configuration).
OK. Thank you.
But, the target is DDR3(1.5V).
> Nevertheless, considering the A4 case regarding 3.3V, note,
>maximum GPIO and VDD_HIGH_IN supply voltage (Absolute Maximum Ratings) is 3.6V ; this
>allows to decrease the SW2 output below 3.3V as soon as possible after boot for reliable
>operation.
OK. I got it.
Best Regards,
Keita