Hello,
According to Table 2-7 (Oscillator and clock recommendations) of the
"Hardware Development Guide ", XTALI VIL and VIH voltage levels, in the
latest i.MX6 series datasheet concern with External megahertz source,
If feeding an external clock into the device.
For oscillator :
"Connect a fundamental-mode crystal between XTALI
and XTALO. An 80 Ω typical ESR crystal rated for a
maximum drive level of 250 μW is acceptable.
Alternately, a 50 Ω typical ESR crystal rated for a
maximum drive level of 200 μW may be used. See the
engineering bulletin EB830 on www.freescale.com for
additional options."
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------