About LVDS output resolution of i.MX 6Quad.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About LVDS output resolution of i.MX 6Quad.

Jump to solution
2,405 Views
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

Is i.MX6Q possible to output the timing of "800(H)x1280(V)" via LVDS?

Refer to attached detail file.

(i.e. I'd like to know the maximum size with horizontal line.)

Best Regards,

Keita

Labels (6)
0 Kudos
Reply
1 Solution
2,249 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes possible, LDB has limitation only on perfomance IMX6DQRM

39.4.1 Input Parallel Display Ports:

For single input data interface case: Up to 170 MHz pixel clock (WUXGA

1920x1200)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
2,250 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes possible, LDB has limitation only on perfomance IMX6DQRM

39.4.1 Input Parallel Display Ports:

For single input data interface case: Up to 170 MHz pixel clock (WUXGA

1920x1200)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,249 Views
keitanagashima
Senior Contributor I

Dear Igor,

Hello.

Thank you for your reply.

>For single input data interface case: Up to 170 MHz pixel clock (WUXGA 1920x1200)

I think that i.MX6 support up to 170 MHz (up to UXGA) in Dual Channel.

Refer to attached file again.

We'd like to use the resolution of 800(H) x 1280(V).

Is it possible to use the display of 1280 vertical lines.

[This is over the 1920(H) x 1200(V)]

Best Regards,

Keita

0 Kudos
Reply
2,249 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes possible.

Best regards

igor

0 Kudos
Reply