About LVDS output resolution of i.MX 6Quad.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About LVDS output resolution of i.MX 6Quad.

跳至解决方案
2,512 次查看
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

Is i.MX6Q possible to output the timing of "800(H)x1280(V)" via LVDS?

Refer to attached detail file.

(i.e. I'd like to know the maximum size with horizontal line.)

Best Regards,

Keita

标签 (6)
0 项奖励
回复
1 解答
2,356 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes possible, LDB has limitation only on perfomance IMX6DQRM

39.4.1 Input Parallel Display Ports:

For single input data interface case: Up to 170 MHz pixel clock (WUXGA

1920x1200)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,357 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes possible, LDB has limitation only on perfomance IMX6DQRM

39.4.1 Input Parallel Display Ports:

For single input data interface case: Up to 170 MHz pixel clock (WUXGA

1920x1200)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,356 次查看
keitanagashima
Senior Contributor I

Dear Igor,

Hello.

Thank you for your reply.

>For single input data interface case: Up to 170 MHz pixel clock (WUXGA 1920x1200)

I think that i.MX6 support up to 170 MHz (up to UXGA) in Dual Channel.

Refer to attached file again.

We'd like to use the resolution of 800(H) x 1280(V).

Is it possible to use the display of 1280 vertical lines.

[This is over the 1920(H) x 1200(V)]

Best Regards,

Keita

0 项奖励
回复
2,356 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes possible.

Best regards

igor

0 项奖励
回复