About LCDIF Timing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About LCDIF Timing

Jump to solution
2,194 Views
x10
Contributor V

Hi,

I get confused about definitions of variables in Fig 33-11 and Fig 33-12 LCD Interface Signals in MPU Write/Read Mode (iMX28 RM rev2 p.2455).

1. Are the TCS and TCH refer to CMD_SETUP and CMD_HOLD in register HW_LCDIF_TIMING respectively?

2. Are the TDSR and TDHR refer to DATA_SETUP and DATA_HOLD in register HW_LCDIF_TIMING respectively?

3. Where can I find the definitions of W1, W2, and W3?

Please let me know if available, Thanks!

BR

Cheng Shi

Labels (1)
0 Kudos
Reply
1 Solution
2,014 Views
arthur_lai
Senior Contributor II

Hi Cheng Shi,

The answers for question 1 and 2 are yes.

TCS and TCH refer to CMD_SETUP and CMD_HOLD in register HW_LCDIF_TIMING respectively.

TDSR and TDHR refer to DATA_SETUP and DATA_HOLD in register HW_LCDIF_TIMING respectively.

W1, W2, and W3 are governed by other timings and do not need to be configured.

Thanks,

Arthur

View solution in original post

0 Kudos
Reply
2 Replies
2,015 Views
arthur_lai
Senior Contributor II

Hi Cheng Shi,

The answers for question 1 and 2 are yes.

TCS and TCH refer to CMD_SETUP and CMD_HOLD in register HW_LCDIF_TIMING respectively.

TDSR and TDHR refer to DATA_SETUP and DATA_HOLD in register HW_LCDIF_TIMING respectively.

W1, W2, and W3 are governed by other timings and do not need to be configured.

Thanks,

Arthur

0 Kudos
Reply
2,014 Views
x10
Contributor V

Thanks Arthur,

I have finished the driver of LCDIF as a parallel bus with right timing.

BR

Cheng Shi

0 Kudos
Reply