About IMX8MQ uboot display LOGO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About IMX8MQ uboot display LOGO

3,845 Views
Joe_C
Contributor I

I have initialized the MIPI DSI controller, and I can see the clock, data and other waveforms through the oscilloscope, but the logo still cannot be displayed, what should I do?Through debugging, I found that the program called the Splash Screen part of the code, instead of LCD_LOGO.

code1.png

0 Kudos
Reply
5 Replies

3,840 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

Did you set panel in uboot? As the screenshot shown, default planel is Hannstar-XGA.

setenv panel xxx

 

BR

Zhiming

0 Kudos
Reply

3,830 Views
Joe_C
Contributor I

My question is that Mipi Lane can measure the waveform, but there is no data. What should I do next?

0 Kudos
Reply

3,822 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Which bsp and soc you are using?

0 Kudos
Reply

3,806 Views
Joe_C
Contributor I

soc:imx8mq

version:4.19.35

Tags (1)
0 Kudos
Reply

3,544 Views
myy
Contributor II

Hi

How do you inited mipi dsi controller? can you give me some help?

0 Kudos
Reply