About IMX6Solo IBIS model.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About IMX6Solo IBIS model.

Jump to solution
1,732 Views
takashitakahash
Contributor III

Hi community.

Our customer has below question.Would you please advice.

Customer will use the EIM terminal to communication of data and the address of the FLASH ROM.

IBIS model such as described on

[Model Selector] gpio in IBIS model

gpio3p3_ds100_sr100_mio GPIO, 3.3V, extra drive, fast sr, slow fsel.

Please advice me , Whether the numerical value of this ds and sr that corresponds to  the value of the register set of Application Manual or Data sheets?

Labels (1)
0 Kudos
Reply
1 Solution
1,653 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

please look at descriptions in

sect.9.5.2 [Model Selector] gpio i.MX6 System Development User’s Guide

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

sect.36.4.258 Pad Control Register (IOMUXC_SW_PAD_CTL_PAD_EIM_RW)

i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,654 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

please look at descriptions in

sect.9.5.2 [Model Selector] gpio i.MX6 System Development User’s Guide

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

sect.36.4.258 Pad Control Register (IOMUXC_SW_PAD_CTL_PAD_EIM_RW)

i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply