About I2C DC Parameters

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About I2C DC Parameters

2,308 Views
goto11
Contributor III

Hello,community


GPIO DC Parameters are listed in Table 29 of the data sheet.
When I2C1_SDA is selected, is DC Parameters VOH / VOL in Table 29 when sending data and VIH / VIL in Table 29 when receiving data?
Or will it switch to open collector when sending data?
Please tell me the VOH / VOL of DC Parameters in that case.

Best Regards,

Goto

Labels (1)
0 Kudos
Reply
3 Replies

2,236 Views
igorpadykov
NXP Employee
NXP Employee

Hi Goto

yes for i2c DC Parameters VOH / VOL are given in Table 29.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,236 Views
goto11
Contributor III

Hello,

Reference material is described in i.MX 7 Dual Applications Processor Reference Manual.
The I2C Bus Specification, Version 2.1, by Philips Semiconductor

The electrical characteristics in the following materials include min0V and max0.4V in the VOL of LOW level output voltage (open drain or open collector) at 3 mA sink current.
References: THE I 2C-BUS SPECIFICATION VERSION 2.1 JANUARY 2000

Isn't the output when I.C I2C interface is selected open drain or open collector output?
If it is an open drain or open collector output, isn't the output characteristic defined only for VOL?

Best Regards,

Goto

0 Kudos
Reply

2,236 Views
igorpadykov
NXP Employee
NXP Employee

>If it is an open drain or open collector output, isn't the output characteristic defined only for VOL?

right.

Best regards
igor

0 Kudos
Reply