About HAB function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About HAB function

1,709件の閲覧回数
baiaaren
Contributor II

Hi,

I find i.MX_Linux_Release_Notes.pdf. Does imx6qp support HAB function?

Thanks

Aaren

ラベル(1)
0 件の賞賛
返信
1 返信

1,579件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Aaren

yes it is supported, one can look at uboot definitions

mx6_common.h  : #ifdef CONFIG_MX6QP #define CONFIG_MX6Q

mx6sabre_common.h  : define CONFIG_SECURE_BOOT

uboot-imx.git - Freescale i.MX u-boot Tree

HAB is almost the same as i.MX6Q, differencies can be found in EB810

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信