About GPIO1 source INT0-INT7 interrupt requests

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About GPIO1 source INT0-INT7 interrupt requests

775 Views
goto11
Contributor III

Hello,community

Is the correspondence between INT7 to INT0 and GPIO1pin from IRQ56 to IRQ63 in Table 7-1 as follows?


IRQ56 INT7 ・・・GPIO1_IO07pin
IRQ57 INT6 ・・・GPIO1_IO06pin
...
IRQ63 INT0 ・・・GPIO1_IO00pin


Is the interrupt with the higher priority the smaller the IRQ number?

Best Regards,
Goto

Labels (1)
0 Kudos
Reply
1 Reply

700 Views
igorpadykov
NXP Employee
NXP Employee

Hi Goto

your understanding about correspondence is correct.

Also yes, interrupt with the higher priority the smaller the IRQ number.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply