About GPIO1 source INT0-INT7 interrupt requests

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About GPIO1 source INT0-INT7 interrupt requests

829件の閲覧回数
goto11
Contributor III

Hello,community

Is the correspondence between INT7 to INT0 and GPIO1pin from IRQ56 to IRQ63 in Table 7-1 as follows?


IRQ56 INT7 ・・・GPIO1_IO07pin
IRQ57 INT6 ・・・GPIO1_IO06pin
...
IRQ63 INT0 ・・・GPIO1_IO00pin


Is the interrupt with the higher priority the smaller the IRQ number?

Best Regards,
Goto

ラベル(1)
0 件の賞賛
返信
1 返信

754件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Goto

your understanding about correspondence is correct.

Also yes, interrupt with the higher priority the smaller the IRQ number.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信