About EIM wait setting in i.MX6DL.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About EIM wait setting in i.MX6DL.

Jump to solution
1,284 Views
keitanagashima
Senior Contributor I

Dear Sir or Madam,

I have a question about EIM wait setting in i.MX6DL.

And I'd like to use the synchronous access on EIM.

[Q1]

Refer to EIM_CSnRCR1 field descriptions in MCIMX6SDLRM(Rev.1).

There is following description about RWSC(Read Wait State Control).

"start of an access"

Is it meaning of "The first rising-edge of BCLK"?

[Q2]

Refer to "Figure 22-12. SRD=1,BCD=0,BCS=0,RWSC=1,RADVA=0,RADVN=0,RFL=0,RL=0" in MCIMX6SDLRM(Rev.1).

When setting to RFL=1, where does the setting of RWSC correspond to in the Figure 22-12?

(It is difficult to understand Figure 22-12. It has mixed internal signal and external signals.)

[Q3]

Refer to Table 22-2 in MCIMX6SDLRM(Rev.1).

There is following description.

"NOTE: For burst devices, WAIT output should be configured to change one cycle before data is ready (before delay)"

This meaning is fixed 1 BCLK before data is ready, isn't it?

Keita

Labels (3)
0 Kudos
Reply
1 Solution
1,073 Views
Yuri
NXP Employee
NXP Employee

Please look at my comments below.

1.
> There is following description about RWSC(Read Wait State Control).

> "start of an access"

> Is it meaning of "The first rising-edge of BCLK"?

Correct.


2.

On the Figure 22-12 there are three BCLK cycles between data sampling

and start of the access. For RFL=1, RWSC indicates when the data is ready for
sampling by the EIM. This means data should be sampled at the rising edge of the
second cycle for RWSC=1. Really figure 22-12 shows diagram for RFL=0, that is, RWSC
bit field indicates when the EIM should start sampling WAIT (READY) signal. So three cycles
are as following : one cycle – start WAIT testing, one cycle - WAIT is OK (ready),
one cycle – read data.

3.
> "NOTE: For burst devices, WAIT output should be configured to change one cycle before data
> is ready (before delay)"

> This meaning is fixed 1 BCLK before data is ready, isn't it?

Yes.

View solution in original post

0 Kudos
Reply
1 Reply
1,074 Views
Yuri
NXP Employee
NXP Employee

Please look at my comments below.

1.
> There is following description about RWSC(Read Wait State Control).

> "start of an access"

> Is it meaning of "The first rising-edge of BCLK"?

Correct.


2.

On the Figure 22-12 there are three BCLK cycles between data sampling

and start of the access. For RFL=1, RWSC indicates when the data is ready for
sampling by the EIM. This means data should be sampled at the rising edge of the
second cycle for RWSC=1. Really figure 22-12 shows diagram for RFL=0, that is, RWSC
bit field indicates when the EIM should start sampling WAIT (READY) signal. So three cycles
are as following : one cycle – start WAIT testing, one cycle - WAIT is OK (ready),
one cycle – read data.

3.
> "NOTE: For burst devices, WAIT output should be configured to change one cycle before data
> is ready (before delay)"

> This meaning is fixed 1 BCLK before data is ready, isn't it?

Yes.

0 Kudos
Reply