About Cortex-M4 in i.MX7 Software Video Encode Capability

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About Cortex-M4 in i.MX7 Software Video Encode Capability

ソリューションへジャンプ
2,979件の閲覧回数
george
Senior Contributor II

Dear all,

Currently, we have planned the product for the image analysis used i.MX7.

We use CA7 only for analysis, and CM4 does mpeg encoding(mpeg) of the input from parallel Camera, and then passes it as UVC to PC.

What performance is mpeg encode of VGA size in the above application using CM4?

What frame rate can be processed?

If there are benchmarks which is reference, please let me know.

Best Regards,

George

ラベル(4)
0 件の賞賛
返信
1 解決策
2,565件の閲覧回数
art
NXP Employee
NXP Employee

The CM4 core of i.MX7 series processors has not enough performance for such a complicated and resource-intensive task as on-the-fly mpeg encoding. So, no benchmark metering has ever been performed for such a case.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

4 返答(返信)
2,566件の閲覧回数
art
NXP Employee
NXP Employee

The CM4 core of i.MX7 series processors has not enough performance for such a complicated and resource-intensive task as on-the-fly mpeg encoding. So, no benchmark metering has ever been performed for such a case.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,565件の閲覧回数
george
Senior Contributor II

Dear Artur,

Thank you for the reply.

We understood your advice.

But I think that we need to try it.

Please tell, if you have the information which is a help to for it.

For example, is there any sample code to refer?

Best Regards,

George

0 件の賞賛
返信
2,565件の閲覧回数
art
NXP Employee
NXP Employee

Unfortunately, no, there is no such a reference code and no any estimation for such a task.

0 件の賞賛
返信
2,565件の閲覧回数
george
Senior Contributor II

Thanks,

George

0 件の賞賛
返信