About CSC(Color Space Conversion) in eLCDIF / i.MX8M

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About CSC(Color Space Conversion) in eLCDIF / i.MX8M

ソリューションへジャンプ
2,562件の閲覧回数
george
Senior Contributor II

Hi all,

 

Our product uses MIPI-LCD via eLCDIF.

We see slight color deviation depending on the type of LCD panel.

According to the reference manual, it seems that the CSC of eLCDIF can be used.

However, I couldn't find the implementation in the current BSP.

I would like to set the coefficients in the LCDIF_CSC_COEFF0 ~ LCDIF_CSC_COEFF4 registers, so please tell me the calculation formula for deriving the coefficient.

 

Best Regards,

George

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,554件の閲覧回数
b36401
NXP Employee
NXP Employee

These registers are described in chapters 13.2.5.18 to 13.2.5.22 "RGB to YCbCr 4:2:2 CSC CoefficientX Register (LCDIF_CSC_COEFFX)" of i.MX 8M Reference Manual.
And there you can find calculation formula.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,555件の閲覧回数
b36401
NXP Employee
NXP Employee

These registers are described in chapters 13.2.5.18 to 13.2.5.22 "RGB to YCbCr 4:2:2 CSC CoefficientX Register (LCDIF_CSC_COEFFX)" of i.MX 8M Reference Manual.
And there you can find calculation formula.

0 件の賞賛
返信
2,548件の閲覧回数
george
Senior Contributor II

Dear @b36401,

 

I apologize for not looking closely at RM.

As you say, I found a description of the formula in each register description. 

 

Thanks,

George

タグ(1)
0 件の賞賛
返信