About CSC(Color Space Conversion) in eLCDIF / i.MX8M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About CSC(Color Space Conversion) in eLCDIF / i.MX8M

Jump to solution
2,564 Views
george
Senior Contributor II

Hi all,

 

Our product uses MIPI-LCD via eLCDIF.

We see slight color deviation depending on the type of LCD panel.

According to the reference manual, it seems that the CSC of eLCDIF can be used.

However, I couldn't find the implementation in the current BSP.

I would like to set the coefficients in the LCDIF_CSC_COEFF0 ~ LCDIF_CSC_COEFF4 registers, so please tell me the calculation formula for deriving the coefficient.

 

Best Regards,

George

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,556 Views
b36401
NXP Employee
NXP Employee

These registers are described in chapters 13.2.5.18 to 13.2.5.22 "RGB to YCbCr 4:2:2 CSC CoefficientX Register (LCDIF_CSC_COEFFX)" of i.MX 8M Reference Manual.
And there you can find calculation formula.

View solution in original post

0 Kudos
Reply
2 Replies
2,557 Views
b36401
NXP Employee
NXP Employee

These registers are described in chapters 13.2.5.18 to 13.2.5.22 "RGB to YCbCr 4:2:2 CSC CoefficientX Register (LCDIF_CSC_COEFFX)" of i.MX 8M Reference Manual.
And there you can find calculation formula.

0 Kudos
Reply
2,550 Views
george
Senior Contributor II

Dear @b36401,

 

I apologize for not looking closely at RM.

As you say, I found a description of the formula in each register description. 

 

Thanks,

George

Tags (1)
0 Kudos
Reply