About Boot Configuration of i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About Boot Configuration of i.MX6

4,517 Views
okamotosatoshi
Contributor IV

Hello.

I want to check about i.MX6Q.

Thank you to answer the following questions.

①BOOT_CFG1[4] ("Override Pad Settings")

Do you match in recognition of the following ?

Set "0" - To use the settings of the config terminal.(GPIO)

Set "1" - To use the settings of PAD_SETTINGS register.

②BOOT_CFG1[4] ("Override Pad Settings")

The use of the setting PAD_SETTINGS register , do you when you select the "toggle mode NAND" in BT_TOGGLEMODE?

③BOOT_CFG2[7:5] ("Toggle Mode - Latency")

What should be selected if you have selected the "raw NAND" in "BT_TOGGLEMODE"?

④BOOT_CFG2[4:3] ("Boot Search Count")

Please tell me how to use it.

What do a setting to do what for the condition?

⑤Fusemap

There is a difference by BOOT_CFG1 [1:0] in P359 "Table 5-9.NAND Boot Fusemap" and P411 "Table 8-11.NAND Boot eFUSE Descriptions".

Which is correct ?

Regards,

-okamoto

Labels (1)
Tags (3)
0 Kudos
Reply
8 Replies

2,746 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

①BOOT_CFG1[4] ("Override Pad Settings")

Do you match in recognition of the following ?

Set "0" - To use the settings of the config terminal.(GPIO)

Set "1" - To use the settings of PAD_SETTINGS register.

[Qiang] when this is 0, the boot rom will use default setting for NAND related pins in registers IOMUXC_SW_PAD_CTL_PAD_NAND_xxx will be set to their default value as iMX6 reference manual described. When this is 1, these IOMUXC_SW_PAD_CTL_PAD_NAND_xxx registers will be set to PAD_SETTINGS values in fuse.

②BOOT_CFG1[4] ("Override Pad Settings")

The use of the setting PAD_SETTINGS register , do you when you select the "toggle mode NAND" in BT_TOGGLEMODE?

[Qiang] "Override Pad Settings" has no business with "toggle mode NAND".

③BOOT_CFG2[7:5] ("Toggle Mode - Latency")

What should be selected if you have selected the "raw NAND" in "BT_TOGGLEMODE"?

[Qiang] "Toggle Mode - Latency" only apply to toggle mode NAND. The delay value should be checked from the customer NAND's datasheet.

④BOOT_CFG2[4:3] ("Boot Search Count")

Please tell me how to use it.

What do a setting to do what for the condition?

[Qiang] How many FCB copies in NAND can be searched by boot ROM, based on Freescale default BSP, it is 4. To define 8 Search Count, the board will be more strong to avoid boot failure, of cource, you also need programe 8 FCBs into the NAND.

⑤Fusemap

There is a difference by BOOT_CFG1 [1:0] in P359 "Table 5-9.NAND Boot Fusemap" and P411 "Table 8-11.NAND Boot eFUSE Descriptions".

Which is correct ?

[Qiang] After checked the boot ROM source code, P411 is correct, 00 - 3; 01 - 2; 10 - 4; 11 - 5. It is a document issue.

0 Kudos
Reply

2,746 Views
okamotosatoshi
Contributor IV

Hi, Qiang

Thank you for reply.

①:Was understood to choose PAD_SETTINGS setting of the fuse or settings register.

②:Was understood that there is no relation to the setting of BT_TOGGLEMODE.

③:was understood to set the delay value when selected the "toggle mode NAND".

  If you select the "raw NAND", What should I set ?

④:I was able to understand a little .

⑤:was  understood the contents of the P411 is correct.

Regards,

-okamoto

0 Kudos
Reply

2,746 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

For the "Boot Search Count", it depends on the programed NAND layout.

For example, based on Freescale default BSP, this value is 4. Then on the NAND flash, block 0 ~ 3 will be used to store four copy of FCB, and the Freescale board will set "Boot Search Count" to 4 too, then when iMX6 boot up, the boot ROM will search FCB from block 0 ~ 3 for boot up. If the boot ROM found a valid FCB, it will continue to boot the board. In this case, when time goes on, even though block 0, 1, 2 became bad block, the board still can boot up due to there is still a valid FCB in block 3.

And if you want to set "Boot Search Count" to 8, then you need programe 8 copy of FCB to NAND block 0 ~ 7.


0 Kudos
Reply

2,746 Views
okamotosatoshi
Contributor IV

Hi, Qiang

Thank you for reply.

There is a question of "Override Pad Settings" of BOOT_CFG1 [4].

If set to "1", "Use PAD_SETTINGS value" is selected .

At this time, I think that "PAD_SETTINGS [5:0]" of "Address:0x6d0" is reflected.

To set the PAD_SETTINGS to blow fuses?

Also, setting value reflects a common setting (Slew Rate/Drive Strength/Speed Settings) for each IOMUXC_SW_PAD_CTL_PAD_NAND_xxx?

Regards,

-okamoto

0 Kudos
Reply

2,746 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

The PAD_SETTINGS fuse is a common setting for all IOMUXC_SW_PAD_CTL_PAD_NAND_xxx pins.

0 Kudos
Reply

2,746 Views
okamotosatoshi
Contributor IV

Hi, Qiang

Thank you for reply.

Advice was very helpful.

Reply also fast and I thank sincerely.

Regards,

0 Kudos
Reply

2,746 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

For ③, when "raw NAND" was used, the delay value can be set to default value 000, they are not used.

0 Kudos
Reply

2,746 Views
okamotosatoshi
Contributor IV

Hi, Qiang

Thank you for reply.

Advice was very helpful.

Reply also fast and I thank sincerely.

Regards,

-okamoto

0 Kudos
Reply