Abnormal display screen

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Abnormal display screen

7,504 Views
hankwang
Contributor V

Hello, we are using BSP 6.6.23_2.0.0 and 6.6.36_2.1.0 and browsers of qtwebengine on the https://jsfiddle.net/92Wc8/3/ and https://www.filestash.app/ websites. The display is abnormal.

Attached is our test file. You can see the code move to the middle of the screen.

And test board is 8MP EVK board.

We also tried boot2qt on the 8MP EVK board. But we don't see this problem. We think that the NXP patch may have an impact on the screen display.

 

 

 

Labels (1)
0 Kudos
Reply
21 Replies

2,231 Views
AshrithaS
Contributor I

Hello hankwang

As u have mentioned that u have tried boot2qt in i.MX8MP.

So, Can u suggest me the proper steps to test boot2QT in i.MX8MP

Regards

Ashritha

0 Kudos
Reply

2,214 Views
hankwang
Contributor V
0 Kudos
Reply

2,183 Views
AshrithaS
Contributor I

Dear @hankwang 

I am following the steps provided in the website, but i am facing issue while giving bitbake command.

Below provided is the error i am getting while giving bitbake command

iwave@iwave-Precision-3460:~/PROJECTS/Boot2qt$ mkdir yocto-boot2qt
iwave@iwave-Precision-3460:~/PROJECTS/Boot2qt$
iwave@iwave-Precision-3460:~/PROJECTS/Boot2qt$
iwave@iwave-Precision-3460:~/PROJECTS/Boot2qt$ cd yocto-boot2qt/
iwave@iwave-Precision-3460:~/PROJECTS/Boot2qt/yocto-boot2qt$
iwave@iwave-Precision-3460:~/PROJECTS/Boot2qt/yocto-boot2qt$
iwave@iwave-Precision-3460:~/PROJECTS/Boot2qt/yocto-boot2qt$
iwave@iwave-Precision-3460:~/PROJECTS/Boot2qt/yocto-boot2qt$ repo init -u https://code.qt.io/yocto/boot2qt-manifest -m v6.9.1.xml
Downloading Repo source from https://gerrit.googlesource.com/git-repo

Your identity is: ashritha.shrinivasa <ashritha.shrinivasa@iwave-global.com>
If you want to change this, please re-run 'repo init' with --config-name

repo has been initialized in /home/iwave/PROJECTS/Boot2qt/yocto-boot2qt
iwave@iwave-Precision-3460:~/PROJECTS/Boot2qt/yocto-boot2qt$ repo sync
Fetching: 100% (13/13), done in 1m35.354s
Checking out: 100% (13/13), done in 0.352s
repo sync has finished successfully.
iwave@iwave-Precision-3460:~/PROJECTS/Boot2qt/yocto-boot2qt$
iwave@iwave-Precision-3460:~/PROJECTS/Boot2qt/yocto-boot2qt$ sync
iwave@iwave-Precision-3460:~/PROJECTS/Boot2qt/yocto-boot2qt$ DISTRO=fsl-imx-xwayland MACHINE=imx8mp-lpddr4-evk source setup-environment.sh -b build-imx8mp-boot2qt
You had no conf/local.conf file. This configuration file has therefore been
created for you from /home/iwave/PROJECTS/Boot2qt/yocto-boot2qt/sources/meta-boot2qt/meta-boot2qt-distro/conf/templates/default/local.conf.sample
You may wish to edit it to, for example, select a different MACHINE (target
hardware).

The Yocto Project has extensive documentation about OE including a reference
manual which can be found at:
https://docs.yoctoproject.org

For more information about OpenEmbedded see the website:
https://www.openembedded.org/


### Shell environment set up for builds. ###

You can now run 'bitbake <target>'

Common targets are:
b2qt-embedded-qt6-image
meta-toolchain-b2qt-embedded-qt6-sdk

QBSP target is:
meta-b2qt-embedded-qbsp

For creating toolchain or QBSP for Windows, set environment variable before running bitbake:
SDKMACHINE=x86_64-mingw32

For more information about Boot to Qt, see https://doc.qt.io/QtForDeviceCreation/

iwave@iwave-Precision-3460:~/PROJECTS/Boot2qt/yocto-boot2qt/build-imx8mp-boot2qt$ sync
iwave@iwave-Precision-3460:~/PROJECTS/Boot2qt/yocto-boot2qt/build-imx8mp-boot2qt$ sync
iwave@iwave-Precision-3460:~/PROJECTS/Boot2qt/yocto-boot2qt/build-imx8mp-boot2qt$
iwave@iwave-Precision-3460:~/PROJECTS/Boot2qt/yocto-boot2qt/build-imx8mp-boot2qt$ export LANG=en_US.UTF-8
iwave@iwave-Precision-3460:~/PROJECTS/Boot2qt/yocto-boot2qt/build-imx8mp-boot2qt$ bitbake meta-b2qt-embedded-qbsp
Timeout while waiting for a reply from the bitbake server (60s at 16:30:24.287064)
iwave@iwave-Precision-3460:~/PROJECTS/Boot2qt/yocto-boot2qt/build-imx8mp-boot2qt$ bitbake meta-b2qt-embedded-qbsp
NOTE: Reconnecting to bitbake server...
NOTE: No reply from server in 30s (for command setFeatures at 16:31:08.195188)
NOTE: Retrying server connection (#1)... (16:31:38.225840)
NOTE: Reconnecting to bitbake server...
NOTE: No reply from server in 30s (for command setFeatures at 16:32:08.232493)
NOTE: Retrying server connection (#2)... (16:32:38.263132)
NOTE: Reconnecting to bitbake server...
NOTE: Retrying server connection (#3)... (Traceback (most recent call last):
File "/home/iwave/PROJECTS/Boot2qt/yocto-boot2qt/sources/poky/bitbake/lib/bb/main.py", line 489, in setup_bitbake
server_connection = bb.server.process.connectProcessServer(sockname, featureset)
File "/home/iwave/PROJECTS/Boot2qt/yocto-boot2qt/sources/poky/bitbake/lib/bb/server/process.py", line 708, in connectProcessServer
sock.connect(os.path.basename(sockname))
BlockingIOError: [Errno 11] Resource temporarily unavailable
, 16:32:38.264973)
NOTE: Reconnecting to bitbake server...
NOTE: Retrying server connection (#4)... (Traceback (most recent call last):
File "/home/iwave/PROJECTS/Boot2qt/yocto-boot2qt/sources/poky/bitbake/lib/bb/main.py", line 489, in setup_bitbake
server_connection = bb.server.process.connectProcessServer(sockname, featureset)
File "/home/iwave/PROJECTS/Boot2qt/yocto-boot2qt/sources/poky/bitbake/lib/bb/server/process.py", line 708, in connectProcessServer
sock.connect(os.path.basename(sockname))
BlockingIOError: [Errno 11] Resource temporarily unavailable
, 16:32:38.265693)
NOTE: Reconnecting to bitbake server...
NOTE: Retrying server connection (#5)... (Traceback (most recent call last):
File "/home/iwave/PROJECTS/Boot2qt/yocto-boot2qt/sources/poky/bitbake/lib/bb/main.py", line 489, in setup_bitbake
server_connection = bb.server.process.connectProcessServer(sockname, featureset)
File "/home/iwave/PROJECTS/Boot2qt/yocto-boot2qt/sources/poky/bitbake/lib/bb/server/process.py", line 708, in connectProcessServer
sock.connect(os.path.basename(sockname))
BlockingIOError: [Errno 11] Resource temporarily unavailable
, 16:32:43.271993)
NOTE: Reconnecting to bitbake server...
NOTE: Retrying server connection (#6)... (Traceback (most recent call last):
File "/home/iwave/PROJECTS/Boot2qt/yocto-boot2qt/sources/poky/bitbake/lib/bb/main.py", line 489, in setup_bitbake
server_connection = bb.server.process.connectProcessServer(sockname, featureset)
File "/home/iwave/PROJECTS/Boot2qt/yocto-boot2qt/sources/poky/bitbake/lib/bb/server/process.py", line 708, in connectProcessServer
sock.connect(os.path.basename(sockname))
BlockingIOError: [Errno 11] Resource temporarily unavailable
, 16:32:48.278565)
NOTE: Reconnecting to bitbake server...
NOTE: Retrying server connection (#7)... (Traceback (most recent call last):
File "/home/iwave/PROJECTS/Boot2qt/yocto-boot2qt/sources/poky/bitbake/lib/bb/main.py", line 489, in setup_bitbake
server_connection = bb.server.process.connectProcessServer(sockname, featureset)
File "/home/iwave/PROJECTS/Boot2qt/yocto-boot2qt/sources/poky/bitbake/lib/bb/server/process.py", line 708, in connectProcessServer
sock.connect(os.path.basename(sockname))
BlockingIOError: [Errno 11] Resource temporarily unavailable
, 16:32:53.285111)
NOTE: Reconnecting to bitbake server...
NOTE: Retrying server connection (#8)... (Traceback (most recent call last):
File "/home/iwave/PROJECTS/Boot2qt/yocto-boot2qt/sources/poky/bitbake/lib/bb/main.py", line 489, in setup_bitbake
server_connection = bb.server.process.connectProcessServer(sockname, featureset)
File "/home/iwave/PROJECTS/Boot2qt/yocto-boot2qt/sources/poky/bitbake/lib/bb/server/process.py", line 708, in connectProcessServer
sock.connect(os.path.basename(sockname))
BlockingIOError: [Errno 11] Resource temporarily unavailable
, 16:32:58.289778)
ERROR: Unable to connect to bitbake server, or start one (server startup failures would be in bitbake-cookerdaemon.log).

Could u give solution for the same?

Regards,

Ashritha

0 Kudos
Reply

7,339 Views
hankwang
Contributor V

Hey @Zhiming_Liu  Thank you for the information.

We also have the same problem using the boot2qt image on the 8MP EVK board on our side.
We use the boot2qt of Raspberry Pi 4 on the Raspberry Pi board. There is no such problem.
The QT used is 6.7.3 on Raspberry Pi board and 8MP EVK board.

boot2qt : https://doc.qt.io/Boot2Qt/b2qt-how-to-create-b2qt-image.html

command for Raspberry Pi.
export MACHINE=raspberrypi-armv8 source ./setup-environment.sh
bitbake b2qt-embedded-qt6-image

We thought that the same QT 6.7.3 has different results on different boards.
We would think it is an issue with NXP BSP.
what you think?

0 Kudos
Reply

7,310 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

We are waiting for reply from internal team 

Best Regards
Zhiming

0 Kudos
Reply

7,303 Views
hankwang
Contributor V

Thanks for the update. We would be grateful if we could get the results as soon as possible.

0 Kudos
Reply

7,226 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

Please try to set 'export QT_QUICK_BACKEND=software' before launching app.

Or Call QQuickWindow::setSceneGraphBackend() in code

 

Reference: https://doc.qt.io/qt-6/qtquick-visualcanvas-adaptations.html

Best Regards
Zhiming

0 Kudos
Reply

7,215 Views
hankwang
Contributor V

Hey, @Zhiming_Liu this solution can work. But after the Qt performance is changed from hardware to software, the system performance becomes worse.

Is there a solution that can solve this problem and keep the hardware solution instead of software.

Tags (1)
0 Kudos
Reply

7,211 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

Find the root cause and solve it based on hardware render may take serval months, at least one month, they wait for patched GPU library release may take half month. If you can wait, then I can then have the internal team continue the process.

Best Regards
Zhiming

0 Kudos
Reply

7,205 Views
hankwang
Contributor V

@Zhiming_LiuSo far, we can wait. Please help me look into this issue. Thanks.

0 Kudos
Reply

6,303 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello,

Update: The search for a solution is still ongoing.

Best Regards,
Zhiming

0 Kudos
Reply

6,299 Views
hankwang
Contributor V

Thanks for the update.

0 Kudos
Reply

7,340 Views
hankwang
Contributor V

Hey, we tested the site. General computers also have the same information.

hankwang_1-1728963869872.png

 

0 Kudos
Reply

7,315 Views
hankwang
Contributor V

@Zhiming_Liu  Thank you for providing this information.

On our side we tested boot2qt of i.mx8mp on 8mp evk board. QT6.7.3 also has the same problem.
But for the Raspberry Pi 4, we tested boot2qt for the Raspberry Pi board. QT 6.7.3 does not have this problem.

boot2qt:  https://doc.qt.io/Boot2Qt/b2qt-how-to-create-b2qt-image.html
command :
export MACHINE=raspberrypi-armv8 source ./setup-environment.sh
bitbake b2qt-embedded-qt6-image


So we think the same QT 6.7.3 has different results on different evk boards. We believe this is an issue with the NXP EVK BSP.
What do you think?



So we think the same QT 6.7.3 has different results on different evk boards. We believe this is an issue with the NXP EVK BSP.
What do you think?

0 Kudos
Reply

7,366 Views
hankwang
Contributor V

Hey @Zhiming_Liu  Can you replicate this problem?

0 Kudos
Reply

7,352 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

I don't think this is an issue from NXP, there are some issue when access https://jsfiddle.net/92Wc8/3/, but i think this is an issue from website or brower while we can see below log. 

js: Unrecognized feature: 'notifications'.
js: Unrecognized feature: 'payment-handler'.
js: Unrecognized feature: 'persistent-storage'.
js: Unrecognized feature: 'background-sync'.
js: Unrecognized feature: 'ambient-light-sensor'.
js: Unrecognized feature: 'accessibility-events'.
js: Unrecognized feature: 'speaker-selection'.
js: Uncaught (in promise) Error: No ads to show.

 

Sometime the display can be normal.

Image (2).jpg

For another website, there is an error about X-Frame-Options.

js: Unrecognized feature: 'speaker'.
js: Refused to display 'https://demo.filestash.app/' in a frame because it set 'X-Frame-Options' to 'deny'.
js: crbug/1173575, non-JS module files deprecated.

 

The issue could from quicknanobrowser/webengine as it's a demo brower. I also test other websites, no such issue.


Best Regards
Zhiming

0 Kudos
Reply

7,364 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

It's in the process of compiling images, I'll keep updating it when I'm done test.


Best Regards
Zhiming

0 Kudos
Reply

7,430 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

Can you provide test steps?

Best Regards
Zhiming

0 Kudos
Reply

7,419 Views
hankwang
Contributor V

1. Build 8MP BSP EVK image and qtwebengine.(mask meta-browser)

2. Burn the image to sdcard or emmc

3. Use emmc or sdard to boot to the file system

4. Open your browser (quick nano browser) and link to the website I mentioned.

5. For filetash websites, you can move folders by scrolling with the mouse. You can see exception screen..

0 Kudos
Reply

7,420 Views
hankwang
Contributor V

1. Build 8MP BSP EVK image and qtwebengine.

2. Burn the image to sdcard or emmc

3. Use emmc or sdard to boot to the file system

4. Open your browser (quick nano browser) and link to the website I mentioned.

5. For filetash websites, you can move folders by scrolling with the mouse. You can see exception screen..

0 Kudos
Reply