Abnormal Tamper Behavior

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Abnormal Tamper Behavior

1,248 次查看
tsung-chihwang
Contributor III

Hi,

We found this symptom on our target.

It shows different tampered result while boot loader placed into QSPI flash or SD card.

pic_1.png

We also found below result on EVK.

pic_2.png

---------------------------------------------------------------------------------------------------------------------

Below are our basic information.

1. Chip model? iMX6UL
2. BSP version? 3.14.38 6ul ga

3. how the BSP image is deployed to QSPI ? Using the MFGTool

BR,

carter

标记 (1)
0 项奖励
回复
1 回复

1,027 次查看
igorpadykov
NXP Employee
NXP Employee

Hi carter

seems problem may be in qspi programming, one can try

to reset board and check if it reboot fine from qspi.

May be recommended to try latest NXP BSPs:

i.MX Software|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复