ATK Tool Modification - Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ATK Tool Modification - Error

跳至解决方案
2,084 次查看
arumugamramasam
Contributor II

Hi,

I am trying to modify the ATK tool source code using GCC compiler under Linux (not using Cygwin from Windows). First of all I was not able to locate the version of ARM GCC compiler (GCC-4.1 tool chain) for linux as specified in the Application Note AN3985. Hence I have downloaded a previous version form GNUARM site. When I tried to compile using make command, it throws an error message as attached. Kindly help me to resolve this issue. Also if the problem is because of the compiler version, please let me know where I can get the 4.1 version tool chain for Linux.

Thanks,

Arumugam R

0 项奖励
回复
1 解答
1,947 次查看
Yuri
NXP Employee
NXP Employee

Please check if the GNU arm cross compiler is installed and "mentioned" in the  path environment variable.
Somewhat as :

export PATH=$PATH:<path_to_arm-elf-bin>

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,948 次查看
Yuri
NXP Employee
NXP Employee

Please check if the GNU arm cross compiler is installed and "mentioned" in the  path environment variable.
Somewhat as :

export PATH=$PATH:<path_to_arm-elf-bin>

0 项奖励
回复