ASRC in IMX8M Mini SoC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ASRC in IMX8M Mini SoC

3,132件の閲覧回数
sreedhar_appala
Contributor III

Hi,

We are working with IMX8M Mini EVK. I am having a doubt regarding the ASRC.

Is ASRC HW block is present in the IMX8M Mini?

1. From the feature comparison section : https://www.nxp.com/docs/en/application-note/AN12667.pdf

i.MX8M Nano has ASRC and i.MX8 Mini has no ASRC

2. But from the i.MX 8M Mini Applications Processor Reference Manual, SPDIF Rx Clock is fed to ASRC.

Please find the attachment.

3. In the kernel code: sound/soc/fsl/fsl-asrc.c is built into the kernel.

I could not understand this conflict details. Please clarify me whether ASRC is included in IMX8M Mini as internal hw.

Thank you, Sreedhar

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

3,080件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I.MX8mm doesn't have ASRC, maybe the RM has error, fsl-asrc.c is for the board which uses ASRC

0 件の賞賛
返信

3,080件の閲覧回数
sreedhar_appala
Contributor III

Thank you  very much Joan Xie, for quick response.

0 件の賞賛
返信