ASRC in IMX8M Mini SoC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ASRC in IMX8M Mini SoC

3,105 Views
sreedhar_appala
Contributor IV

Hi,

We are working with IMX8M Mini EVK. I am having a doubt regarding the ASRC.

Is ASRC HW block is present in the IMX8M Mini?

1. From the feature comparison section : https://www.nxp.com/docs/en/application-note/AN12667.pdf

i.MX8M Nano has ASRC and i.MX8 Mini has no ASRC

2. But from the i.MX 8M Mini Applications Processor Reference Manual, SPDIF Rx Clock is fed to ASRC.

Please find the attachment.

3. In the kernel code: sound/soc/fsl/fsl-asrc.c is built into the kernel.

I could not understand this conflict details. Please clarify me whether ASRC is included in IMX8M Mini as internal hw.

Thank you, Sreedhar

0 Kudos
Reply
2 Replies

3,053 Views
joanxie
NXP TechSupport
NXP TechSupport

I.MX8mm doesn't have ASRC, maybe the RM has error, fsl-asrc.c is for the board which uses ASRC

0 Kudos
Reply

3,053 Views
sreedhar_appala
Contributor IV

Thank you  very much Joan Xie, for quick response.

0 Kudos
Reply